A safe and reliable alternative in the Australian Outback

Overview_TEXT

Overview

No commodity is more precious in the vast Australian Outback than water, especially on cattle and sheep properties that are measured in thousands of square kilometres. However, Hamilton Downs, a 2,000 km² cattle property 80 km South West of Alice Springs, averages barely 280 mm of rain a year, and relies totally on underground water. Up until now the property has relied on wind power and a supporting diesel generator for a constant water supply. Nevertheless, a large number of windless days and safety issues in connection with the ongoing maintenance of the tall windmills have encouraged the Hamilton Downs Manager, Mr. Jamie Evans, to look for a safer and more efficient alternative.

The Situation

Hamilton Downs runs about 5,000 shorthorn cattle. The original pump installation was operated by a windmill and supported by a diesel generator pumping water from a well 100 m from the homestead. The solution provided water to a holding tank that, in turn, fed stock troughs in three paddocks – the largest of which is 223 km2 in size. While ongoing maintenance and lack of wind have always been key problems associated with wind power, occupational health and safety had become equally critical. Hamilton Downs manager, Mr. Jamie Evans, has become more aware of the dangers his employees face in climbing windmills – problems that are difficult to overcome in a vast land where cranes are a rarity.

The Grundfos Solution

While water is a scarce commodity, sunlight is almost constantly in abundance in the Australian Outback. Therefore, a SQFlex Solar and generator back-up seemed a much more efficient solution for the cattle property in central Australia. But more importantly, the PV solar modules are virtually maintenance-free and much safer to handle than the original windmills. On a trial basis and in conjunction with Grundfos Australia, Territory Pastoral Services installed 12 PV solar modules to power a three-inch helical rotor pump set in the well at a level of 64 m. The solar modules produce a maximum of 546 W and if the sun fails, the generator will be used as a back-up power system.
 

The Outcome

Not only has Hamilton Downs’ new water supply proven very reliable and efficient, Mr. Jamie Evans also emphasises that the SQFlex Solar saves him considerable amounts of time on maintenance and repair: "This is an important factor when it takes a day to do a well check and inspect troughs and stock. That used to be a full time job." In close cooperation with Grundfos Mr. Jamie Evans monitors the efficiency of the system during the trial period and he is very pleased with the potential of the pumps. "We would certainly – when drilling new wells – look at installing SQFlex pumps in future rather than using windmills. They certainly require less maintenance, and are a heck of a lot safer and easier to repair than windmills", says Mr. Evans.


    Facebook Twitter LinkedIn Technorati

Topic:

SQFlex Solar helps Australian cattle farm

Location:

Hamilton Downs, Australia

Company:

An Australian cattle farm

Contacts_TEXT

Contact

If you need a similar solution, please contact us for further information.

Contact

If you need a similar solution, please contact us for further information.

How to Buy_TEXT

How to buy

In this section we will guide you to your country site