Grundfos fits out one of Europe’s largest shopping centres

Overview_TEXT

Overview

Regarded as one of Europe’s largest shopping centres, the Dolce Vita Tejo covers more than one hundred thousand square metres and two spacious areas dedicated to food outlets and entertainment.

The centre, which was opened in May 2009, offers around 300 stores and parking facilities for nine thousand vehicles.

Situated in the municipality of Amadora, the Dolce Vita Tejo boasts the biggest indoor square in Europe, similar in size to Lisbon’s Praça dos Restauradores.

 

Grundfos provided

- Energy savings

- Pumps for a wide range of applications

- Reliability

- Hard-wearing equipment

 

The task

The main priorities when selecting the pumping systems for the shopping centre were to guarantee the highest possible levels of comfort and increased energy efficiency. It was for this reason that Grundfos was selected as one of the suppliers, as the equipment Grundfos presented offered the best value for money, explains Bruno Rodrigues of the Electromechanical Installation Department at Pinto & Cruz, part of the group TEJO – J. J. Tomé – Sousa Pedro – Pinto & Cruz, ACE, the organisation responsible for the special water, electricity, air conditioning and security facilities.

The Grundfos solutions installed in the Dolce Vita Tejo serve a range of areas and needs: HVAC (heating, ventilation and air conditioning), water supply, fire and waste water. "The aim is to distribute water throughout the building while complying with the design and regulatory requirements, as well as to guarantee users a service with the necessary levels of quality and comfort", he explains.

 

The solution

According to the company that performed the installation, the performance of the equipment meets all the requirements. "As a result, we have a functional system whose strengths include energy savings due to the use of speed-variable equipment where consumption can be adjusted when needed. We also must not forget Grundfos’ extensive experience in this field, the high quality of the equipment and the specialist technical team, who are able to respond to any situation", he adds.

 

The result

"To date, I can only say that the drinking water supply pumps, ground water supply for the cooling towers and the irrigation system have worked extremely well, without any fault signals or evidence of performance defects during their intended use. Fortunately we have not been forced to test the fire safety system in practice, however we conducted a few trial runs with excellent results. In general, the equipment supplied by Grundfos has proven to be sturdy and of a high quality, as well as extremely reliable.

With regard to the pumping units linked to the air conditioning system, the excellent performance of the Grundfos pumps provides a sense of confidence and peace of mind. Time spent on corrective maintenance of this equipment is downtime, and the periods in which the equipment is functioning properly therefore equals excellent value for money."

Hugo Prata

Facilities Manager, Dolce Vita Tejo

 

Technical specifications

Name of the building: Dolce Vita Tejo

Architect: Promontório and RTKL.

Promotor: Chamartin Imobiliária and ING Development.

General contractor: Mota-Engil; Somague.

 

Design engineer:

Ductos – Sociedade de Projectos de Engenharia, Lda (water supply, waste water, fire).; LMSA – Engenharia de Edifícios, S.A. (AVAC).

Supervision: Engexpor – Consultores de Engenharia, S.A; FICOPE- Fiscalização, Coordenação e Projectos de Engenharia, Lda.

Installer: TEJO – J. J. Tomé – Sousa Pedro – Pinto & Cruz, ACE.

 

Equipment supplied

HVAC

21 x monocellular centrifugal TP pumps

1 x REFLEXOMAT

4 x SERVITEC MAGCONTROL

4 x REFLEX 600L tanks

 

Floor heating systems

26 x TPED pumps

26 x REFLEX tanks

 

Heat recovery systems

12 x TPED pumps

12 x REFLEX tanks

 

Waste water

17 x SE1 submersible pumps for waste water and their Grundfos consumer units and accessories

 

Water supply

3 x HYDRO MPC systems with speed variation

1 x HYDRO 1000 system

1 x HYDRO MULTI-S system

 

Fire safety

4 x Fire Safety Systems that meet the CEPREVEN standard


    Facebook Twitter LinkedIn Technorati

Topic:

Shopping centre

Location:

Amadora, Portugal

Company:

Dolce Vita Tejo

hydrompc_2
Contacts_TEXT

Contact

If you need a similar solution, please contact us for further information.

Contact

If you need a similar solution, please contact us for further information.

How to Buy_TEXT

How to buy

In this section we will guide you to your country site