Grundfos keeps large flows moving on new stormwater line in Budapest

Overview_TEXT

Overview

The Budapest Sewage Works (BSW) Ltd. – part of the VEOLIA Group – is the biggest public wastewater and environmental protection company in Hungary. BSW provides services in the field of sewage network operation, wastewater treatment, and flood and inland water protection. The company is the leader in the introduction and installation of new environmental technologies and biological waste handling in Hungary.

BSW operates the entire 5400 km long sewage network system and two of the wastewater treatment plants in Budapest. The capital city has 1.7 million inhabitants with large industrial areas which generate more than 0.5 million cubic meters of wastewater per day.

The situation:
A reconstruction and capacity increase was necessary at the Ferencváros Pumping Station – the biggest pumping station in the wastewater system – in connection with the construction works at the Budapest Central Wastewater Treatment Plant. If conditions are dry, 200,000 cubic meters of wastewater is pumped per day to the plant.

The new Ferencváros Pumping Station is a part of a huge environmental protection
investment in Budapest focusing on the Central Wastewater Treatment Plant construction, the collection system and mains construction, and pumping stations that cross the River Danube. When the final stages are completed, 100% of Budapest wastewater will be biologically treated; compared to 95% today.

To ensure that all wastewater passes through treatment processes even in heavy rain or surface flooding events, a bypass stormwater line was required. In 2010, the new pumping station was constructed with the separate stormwater line, on the site of the original wastewater pumping station from 1893. Ten high performance KPL submersible axial-flow stormwater pumps were delivered and installed into the stormwater line by Grundfos.

The Grundfos solution:
The solution presented by Grundfos was 10 vertically-installed submersible axial flow stormwater pumps. These 365 kW pumps are capable of pumping 3018 litres per second at 9.6 meters head. Grundfos pumps were chosen, because the technical details, efficiency, delivery time and price of the pumps met the requirements of the investment committee, which consisted of the operator (BSW) and the construction
company (Colas Alterra).

The outcome
This type of application with its special design and using very large pumps was unique in Hungary. Close cooperation was needed with the designers, the construction company and the operators.
Pumps of this size require specialised technical staff and processes; for example two cranes had to work together for installation because of the heavy weight of the pumps and cables and tight tolerances. After two years operation all the pumps work well without any problems and the customer is satisfied.


    Facebook Twitter LinkedIn

Topic:

Flood control

Location:

Budapest

Company:

Ferencváros pumping station

Contacts_TEXT

Contact

If you need a similar solution, please contact us for further information.

Contact

If you need a similar solution, please contact us for further information.