Grundfos supports Pepsico’s energy conservation drive

Overview_TEXT

Overview

Grundfos supports Pepsico’s energy conservation drive


PepsiCo India Holdings Private Limited is a multinational
company with interests in Manufacturing, Marketing and
Distribution of grain-based snack foods, beverages, and
other products. PepsiCo entered India in 1989 and in a
short period of 23 years has grown into the largest and
one of the fastest growing food & beverage business in the
country. PepsiCo has a commitment on ‘Performance with
Purpose’ to find innovative ways to minimize their impact
on the environment, which primarily focuses on Water and
energy conservation.

 

The Situation

PepsiCo, Roha, Maharashtra, as a part of their initiative
to conservation of energy, invited Grundfos for Energy
Audit. The report showed that the existing pumps were
consuming more energy related to pressure and the
wastage of water was also alarmingly noticeable. So,
PepsiCo, Roha decided to replace few of their existing
critical pumps with ‘energy efficient pumps’.

The Grundfos Solution

The detailed Energy audit report suggested the
replacement with Grundfos Vertical pumps and closed
couple end suction pumps (Models:- CRN 64-2, NB
125-200/221, and NB 100-200/170, CR 20-03, and CR
15-04) in the utility and process systems in order to
optimize the water-energy performance.

The technical Data for CRN/CR pumps are listed below:
Flow rate: max.180m3/h
Head: max 330m
Liquid temperature: -40 °C to +180 °C
Operational pressure: max.33 bar

The technical Data for NB pumps are listed below:
Flow rate: max.1000 m3/h
Head: max 160m
Liquid temperature: -25 °C to +140 °C
Operational pressure: max.25 bar

The Outcome

Grundfos pump solutions thus saved PepsiCo, Roha
5625 kWh units per month amounted to Rs.4,00,000
(approximate) annually.


“Grundfos pumps saved 41 % of energy consumption,
which has contributed greatly towards PepsiCo Roha’s
initiation on Energy Conservation. Grundfos high quality
pumps offer reliability, which is very important to ensure the
quality of production” says a maintenance official.

Features for Grundfos pumps:-
1. Ease of installation and commissioning
2. Trouble free operation
3. Reliable performance

Topic:

The audit results highlighted an over consumption of energy and noticeable water wastage. As a consequence PepsiCo Roha in Maharasta India decided to replace existing critical systems with energy efficient pumps. The energy consumption of the pumpsystem was thereby reduced by 41%.

Location:

Maharasta, India

Company:

PepsiCo Roha

Contacts_TEXT

Contact

If you need a similar solution, please contact us for further information.

Contact

If you need a similar solution, please contact us for further information.

How to Buy_TEXT

How to buy

In this section we will guide you to your country site

How to buy

In this section we will guide you to your country site

Select your country: