Patagonian sun turned into water

Overview_TEXT

Overview

The situation

Large distances are a characteristic factor in the southern end of the Argentinean Patagonia. This makes it a real challenge to install traditional energy sources there. Clean energies solve this problem and many times this kind of solution can evenmake automatic a daily task.

This was exactly the case at San José ranch, located in Guer Aike, 110 km North West from RíoGallegos, Santa Cruz province, Argentina. That is where a family has been working on extensive ovine cattle farming for the last 60 years. This typical Patagonian establishment holds 9.000 sheepin its 36.000 hectares. Production is based on rational usage of natural resources while breedinglivestock in a sustainable way.

The solution

Guided by this way of leading a business, some years ago the owners of San José ranch had invested in renewable energies to get groundwater for cattle drinking. Since then the task is carried on by 3 SQ Flex pumps. Encouraged by the good results, a step further was taken and a CR Flexpump was installed to irrigate a pasture.

The selected CR Flex 5-5 gets the necessary energy from 6 Grundfos solar panels of 100 watts each, connect in series. A Grundfos IO50 controller completes the set up. The pumping system was installed 4 m from the Coyle river bank, with 1 m level difference at the aspiration, where a non-returnvalve was included.

Water thus captured by the CR Flex is driven by the same pump 70 m from the aspiration point andit is used to irrigate by flooding a 2 hectare pasture of Ryegrass.

Previously this task had been done by a pump that had a 4 hour autonomy while using 4 l of petrol. This implied the need of keeping a supply of fuel in the ranch.

The outcome

The complete independence of the new Grundfos pump makes it possible for the pasture to get water during the day without the need of pouring fuel in the old pump and turning it on every day. Today the irrigation is made during daylight hours.

“Now I don´t need a person to go everyday up to the pump to turn iton and I´ve been able to eliminate the cost of fuel to make it work. I´m very satisfied with the flow obtained”, comments Mr. Fernando Barcena, administrator and owner of the ranch. Mr. Fernando Barcena was so pleased that more CR Flex pumps were later acquired for the same establishment.

The dimensioning of the system was made based on the Grundfosonline dimensioning tool. The city chosen for irradiation calculationpurposes was Río Gallegos. A 2 m discharge height was consideredin reference to the pumping system. Software calculations indicated a daily flow of 50.000 l/day during spring and summer, which is the period of irrigation for the pasture.


    Facebook Twitter LinkedIn

Topic:

Renewable energy, clean energy

Location:

Guer Aike, Argentina

Company:

San José ranch

Contacts_TEXT

Contact

If you need a similar solution, please contact us for further information.

Contact

If you need a similar solution, please contact us for further information.