Upgrade kit solves jamming issues in Sweden

Overview_TEXT

Overview

NSVA, a water services company in southern Sweden, moves wastewater from 230,000 inhabitants in a large low-lying area covering six municipalities. At one of the end stations immediately prior to a wastewater treatment plant, the owner decided to replace one of three pumps with a Grundfos SL wastewater pump with a standard channel impeller. The pump jammed regularly and Grundfos was informed of this.

Grundfos acted immediately and replaced the impeller with an S-tube upgrade kit. This was done in January 2012 and the pump has been running ever since with no alarms. The pump is working as the duty pump and takes care of all the water in the pit. The two other pumps are for back-up in the event of heavy rain.





    Facebook Twitter LinkedIn Technorati

Topic:

S-tube upgrade kit solves jamming issues

Location:

Sweden

Company:

NSVA, Sweden

Grundfos supplied:
Pump model: SL1.100.150.75.4.50D.B
Impeller type: S-tube
Installation date: January 2012

Contacts_TEXT

Contact

If you need a similar solution, please contact us for further information.

Contact

If you need a similar solution, please contact us for further information.