SQFlex revives historic Australian outback station

Overview_TEXT

Overview

A century-old sheep and cattle station situated near the Flinders Ranges, 650 km north of Adelaide, is gaining a new lease of life thanks to Grundfos solar powered SQFlex pumps. Mount Lyndhurst Station is a 3,500 km² property, which when fully stocked will run up to 15,000 breeding ewes and 1,500 breeding cattle. Mark and Anne Scammell acquired it some 18 months ago. When purchased, 30 windmills – half of which no longer worked – provided the property’s water supply. The need for water, however, was not reflected in this reduction in output. Rather than repair them, the Scammells decided to replace them all with 17 Grundfos SQFlex Solar pumps.
 

The Situation

The Mount Lyndhurst station was very run down when purchased by Mark and Anne Scammell. This large sheep and cattle station was established in the mid 1870s, but had fallen on hard times. Like many cattle stations of that era, it was extremely labour intensive. Over the past 20 years, however, it failed to maintain pace with modern trends. The Scammells set out to revitalise the station, finding out that the unreliable water supply system needed attention.


The Grundfos Solution

17 Grundfos SQFlex 2.5-2N units are powered by 136 GF 50, 50 W solar modules. Each installation has eight modules on average. IO 101 switch box accompanies them, and each system has replaced a windmill – one of the Australian outback icons. Even though the water depth varied from 9 to 50 m and the flows ranged from 3,000 to 5,000 gallons (11 to 19 m³) a day, the same pump model was flexible enough to cope with this varied demand. Each pump is fitted with the IO 101 switch box, enabling the usage of a generator, if pumping is necessary for additional hours. The systems range from 150 W to 600 W, and all are mounted on a passive gas tracking system so that the sunlight is maxi-mised. The pumps fill water reservoirs then in turn gravity feed water to stock troughs.
 

The Outcome

Mount Lyndhurst Station is now freed from maintaining a large range of spare parts for various different pumps. Additional benefits include the SQFlex’s AISI 316 stainless steel casing, enabling it to cope with the harsh and corrosive nature of the water. Mr. Mark Scammell is very pleased with the result. "Properties such as Mount Lyndhurst operate with as few staff as three or four people. Had we kept the windmills, we would have needed at least two additional staff simply to maintain them. Solar power is the way to go, and the SQFlex pumps offer versatility, great performance, and reliability." "We decided that the expense of installing the Grundfos SQFlex Solar pumps would be a sound investment in the long term. We could either keep and repair the windmills or replace them. The cost of repairing the windmills was going to be $90,000 and as an added benefit, the windmills could be sold as they were, for $30,000. So it became very cost effective to consider solar technology," he states.

Topic:

SQFlex is a cost-effective solution

Location:

Flinders Ranges, Australia

Company:

A century-old sheep and cattle station

Contacts_TEXT

Contact

If you need a similar solution, please contact us for further information.

Contact

If you need a similar solution, please contact us for further information.

How to Buy_TEXT

How to buy

In this section we will guide you to your country site