Swedes cheer teamwork, savings in pressurized wastewater network

Overview_TEXT

Overview

The situation

Sweden’s largest homeowner association faced a challenge. The year was 2012. The area was Lidköping in central Sweden – homes and farms scattered among 100 square-kilometres of rolling hills, lakes, forests and beaches.

“This area is quite typical for the Swedish countryside. Properties are very far apart, and lots of people have their own wells and sewers,” says Jan Magnusson, head of the homeowner association Kållands Vatten & Avloppsförening (Kållands VA) in Lidköping, Sweden.

Much of the area is also in a water protection zone. Swedish law was moving toward requiring all homes in such areas to connect to both municipal water and wastewater networks. Homeowners outside city limits would have to finance and build their own lines, however.

“The municipality would not assume such a responsibility, so it was up to the property owners to solve this problem,” says Jan Magnusson. At the same time, the municipality’s requirements for sewage removal from all properties were strict. Therefore – as is common all over Sweden – Kållands VA formed to tackle the challenge as a group, he explains.

In 2006, it connected water lines from all properties to the municipal utility. The homeowners knew the municipality was going to pressure them for sewage removal, too. So in 2012, Kållands VA decided to add wastewater – a more challenging undertaking.

“We didn’t know the project would be this large when we started,” says Jan Magnusson. “It grew along the way. More and more people got interested as we went along. In the beginning we were just talking about 260-280 properties. We finished with about 670. It was an incredibly large project, indeed,” he says. “And all together we solved the problem. In cooperation with Grundfos, of course.”

 

The solution

Kållands VA asked Grundfos to supply wastewater pumps, but the company did more than that, Jan Magnusson says.

“Grundfos mapped the system and dimensioned the network,” he says. “They made a design for every part and leg, and divided the network into smaller legs. Then they made a map of the entire system and suggested the intermediate pumping stations. And then, of course, the size and dimensions of pumps and pipes.” 

Grundfos specialists at the Grundfos Water Utility Competence Centre used an advanced hydraulic tool called SIMPS – which stands for Simulations of Pressurized Sewer Networks – for sizing and dimensioning the pumps, piping and pumping stations. Grundfos supplied Prefabricated Pumping Stations (PPS) at 530 locations plus 16 larger, intermediate PPS for network pumping stations. In the end, the design incorporated 130 kilometres of piping.

The SEG AutoADAPT grinder pumps in the smaller PPS eliminated the need for extra pump controllers, switches and extra cables, since everything was included inside the pump. This cut installation time in half. “We reduced the overall installation cost by 50%,” says Kjell Asplund of Grundfos Sweden.

The intermediate PPS network stations used SEG and SLV wastewater pumps from 4 kW to 11 kW. This design – with 16 intermediate PPS and small to medium-sized pumps instead of just a few very large pumping stations with high-kilowatt motors – helped to reduce operational costs and energy consumption, he adds.

“It meant that each household could use the smallest pump size possible. And then the smaller pumps in the intermediate PPS saved energy compared to a few PPS with large pumps,” he says.

 

The outcome

It took the association three years to finish the project. “We’ve had very few problems in starting up all these areas,” says Jan Magnusson. “We’ve had very few stops. It’s been incredibly painless to start up the whole thing."

As for the equipment, he adds, they are not complaining.“Right now we’re servicing all the pumps under the guarantee warranty, and we’ve gone over the first nearly 200 pumps. We have not found a single pump with a fault. All of them have been completely fine after working for three years. We consider that really good.”


    Facebook Twitter LinkedIn

Topic:

Grundfos designs pressurised wastewater network for Swedish association, saving time and installation costs

Location:

Lidköping, Sweden

Company:

Kållands Vatten & Avloppsförening

SIMPS (SIMulation of Pressurised Systems) for sizing and dimensioning
SIMPS (SIMulation of Pressurised Systems) for sizing and dimensioning
Contacts_TEXT

Contact

If you need a similar solution, please contact us for further information.

Contact

If you need a similar solution, please contact us for further information.

How to Buy_TEXT

How to buy

In this section we will guide you to your country site