F&B Industry

The global megatrends of climate change, growing populations, increased urbanisation, growth of a new middle class etc. means an unsustainable usage of water in many watersheds. The Food & Beverage industry are not exempt from this equation and therefore face increased legal constraints on water supply, wastewater discharge and higher costs. Furthermore, the industry faces a growing interest from stakeholders in establishing a sustainable operation with regard to water in operation, supply chain and in the local watersheds.

On-site wastewater treatment and re-use: Grundfos BioBooster can provide food and beverage manufacturers with a sustainable treatment of wastewater. This opens up for the opportunity to re-use the water as technical
water either for production or in the local surroundings. This allows for water consumption activities which otherwise could have been hampered.

Our technology treats wastewater for reuse within the actual factory by removing organics and bacteria. The water is re-used in the actual production of food/beverages without jeopardising food safety.

Characteristics:
Being a closed system, the BioBooster treatment plant has no unpleasant odours – they are confined and removed.
The ultrafiltration membranes remove bacteria thereby reducing risks for re-contamination.
Our technology has scalability, this means that we can adapt to the size of your production with large variations in organic and hydraulic loading– now and in the future.

Case story

biobooster-Arla_grundfos_stories_1042-20160511

Danish dairy, Arla Rødkærsbro, treats wastewater onsite and reuses it in production.

See case

Case story

biobooster-Vimmerby-case_DSC_0119

Enabling increased production for Arla Vimmerby.

See case