CUE controllers

End-of-Life Information
Grundfos CU200, CU300 and CU301 controllers must be disposed of according to local regulations by using a public or private waste collection service. If this is not possible, contact the nearest Grundfos company or service workshop.


Safety Risk

Safety related to materials used

  • There is no risk for people during the disassembly process posed by the materials used in the product.

Safety related to handling the product

  • Care should be taken when handling the pump/components due to the weight.

Disassembly of the Product

The main materials of the components are:

  • Polyamide composite
  • Various electronic components
  • Aluminium (only CU200)

CU200, CU300, CU301 controllers can therefore be recycled to a large extend – depending on the national possibilities for recycling.

DesignationNameMaterialSpecial Disassembly Consideration
1Front cover
Front foil
(Electronics)

Polyamide
Polyester (with electronics)
PCB with components

 
2ElectronicsPCB with components 
3Back coverPolyamide 
4Cable entryPolyamide 
5Mounting plate (CU200)Aluminium 
Additional materials:Screws, gaskets etc.: Various materials less than 5% of weight
2a. End-of-Life_CU200 CU300 CU301 controllers
CU200, CU300, CU301 controllers




    Facebook Twitter LinkedIn Technorati