IO controllers

End-of-Life Information
Grundfos IO101 and IO102 controllers must be disposed of according to local regulations by using a public or private waste collection service. If this is not possible, contact the nearest Grundfos company or service workshop.

Safety Risk

Safety related to materials used

  • There is no risk for people during the disassembly process posed by the materials used in the product.

Safety related to handling the product

  • Care should be taken when handling the pump/components due to the weight.

Disassembly of the Product

The main materials of the components are:

  • Polyamide composite
  • Various electronic components
  • Aluminium

IO101 and IO102 controllers can therefore be recycled to a large extend – depending on the national possibilities for recycling.

DesignationNameMaterialSpecial Disassembly Consideration
1 Front cover
Front foil
2SwitchPolyester / Steel 
3Cable entryPolyamide 
4Mounting plateAluminium 
5Back coverPolyamide / Stainless steel 
6RelayPolyester / Cobber 
7Terminal blockPolyester / Steel 
Additional material:Screws, gaskets etc.: Various materials less than 5% of weight.
2b. End-of-Life_IO101 IO102 controllers

    Facebook Twitter LinkedIn Technorati