IOXXX, CUXXX

End-of-Life Information

Grundfos CU211, CU212, CU213, CU214, CU215 and IO111, IO112 and IO113 controllers must be disposed of according to local regulations by using a public or private waste collection service. If this is not possible, contact the nearest Grundfos company or service workshop.

Safety Risk

  • Safety related to materials used
    There is no risk for people during the disassembly process posed by the materials used in the product.
  • Safety related to handling the product
    Care should be taken when handling the pump/components due to the weight.

Disassembly of the Product

The main materials of the components are:

  • Polyamide composite
  • Various electronic components
  • Aluminium

CU211, CU212, CU213, CU214, CU215 and IO111, IO112 and IO113 controllers can therefore be recycled to a large extend – depending on the national possibilities for recycling.   

 

DesignationName  MaterialSpecial Disassembly Consideration
1 Front cover
Front foil
Polyamide
Polyester  
 
2Printed circuit boardGlass fiber, copper, tin 
3ScrewsSteel 
4Printed circuit boardAluminium 
5Back coverPolyamide 
6ScrewsSteel 
Additional materials:  Labels, connector etc.: Various materials less than 5% of weight. 
2b. End of life IOXXX_CUXXX




    Facebook Twitter LinkedIn Technorati