Liftaway B

End-of-Life Information
Grundfos Liftaway B must be disposed of according to local regulations by using a public or private waste collection service. If this is not possible, contact the nearest Grundfos company or service workshop.

Safety Risk

  • Safety related to materials used
    There is no risk for people during the disassembly process posed by the materials used for the product.
  • Safety related for handling the product
    Caution is required when accessing the inside of the tank as it may be toxic caused by the waste water.
     

Disassembly of the Product
The main materials of the components are:

  • Polyethylene (PE)
  • Iron
  • Aluminium

and can therefore be recycled to a large extend – depending on the national possibilities for recycling.

There are no tools required to disassemble the product. The tank can be equipped with a variety of pumps. Please refer to the corresponding information.

DesignationName  MaterialSpecial Disassembly Consideration
1CoverAluminium 
2Drain gratingStainless steel 
3TankPolyethylene (PE)Caution is required when accessing the inside of the tank as it may be toxic caused by the waste water
4Telescopic partPolyethylene (PE) 
5c Liftaway_B




    Facebook Twitter LinkedIn Technorati