Liftaway C

End-of-Life Information
Grundfos Liftaway C must be disposed of according to local regulations by using a public or private waste collection service. If this is not possible, contact the nearest Grundfos company or service workshop.

Safety Risk

  • Safety related to materials used
    There is no risk for people during the disassembly process posed by the materials used for the product.
  • Safety related for handling the product
    Caution is required when accessing the inside of the tank as it may be toxic caused by the waste water.


Disassembly of the Product

The main materials of the product is:

  • Polypropylene (PP)

and can therefore be recycled to a large extend – depending on the national possibilities for recycling.

There are no tools required to disassemble the product. The tank can be equipped with a Grundfos Unilift KP pump. Please refer to the corresponding information.

DesignationName  MaterialSpecial Disassembly Consideration
1CoverPolypropylene (PP) 
2TankPolypropylene (PP) 
5d Liftaway_C

    Facebook Twitter LinkedIn Technorati