End-of-Life Information

Grundfos MTS pumps must be disposed of according to local regulations by using a public or private waste collection service. If this is not possible, contact the nearest Grundfos company or service workshop.

Safety Risk

Safety related to materials used

  • There is no risk for people during the disassembly process posed by the materials used in the product.
  • Be sure that the pump is clean and empty for liquid before disassembly.

Safety related to handling the product

  • Care should be taken when handling the pump/components due to the weight.

Disassembly of the Product

The main materials of the components are:

  • Cast iron
  • Stainless steel
  • FKM rubber

The MTS pump can therefore be recycled to a large extend – depending on the national possibilities for recycling. To disassemble an MTS pump, standard tools can be used.

DesignationName  MaterialSpecial Disassembly Consideration
APump coverCast iron 
BDischarge casingCast iron 
CShaft seal Stainless steel (1.4571)
Seal rings: Silicon carbide / Silicon carbide
DScrewsHardened steel 
ERotor housingCast iron 
FSuction casingCast iron 
Additional materials:  Screws, gaskets etc.: Various materials less than 5% of the weightScrews, gaskets etc.: Various materials less than 5% of the weight
5i. MTS_TM061770

    Facebook Twitter LinkedIn Technorati