Information on changes in the latest version of WebCAPS
What's new in WebCAPS 2012.03?
Software
Renewable:
- Problems with to high temperatures when defining custom solar panels are now corrected.
- Removed Hz in renewable report
- Added restriction on max number of solar panels determined from the Pmax value for the pump
- Changed the ”limit search” i sizing so it’s not as restrictive
Other changes
- Problems with missing buttons when starting WebCAPS on an IPad is now solved.
- Allow variant configuration checkbox added in catalogue. By enabling / disabling it’s now possible to control if only products with P/N should be part of the result or ”On request” products should be available too.
- Literature download error for some products was solved.
Data
New products:
- RCME, Rainwater pumping system
- IO50
- SE/SL 9-30 kW
What's new in WebCAPS 2012.02?
Software
- Replacement problem regarding getting replacements for CRNE and CHI pumps are solved
- English text appears together with local language in Service is now solved
- 3 duty point sizing available for Waste Water pumps
- CAD description added to SPK products so it's possible to distinguish between different types
- Load profile in PDF not matching the one displayed in CAPS is now solved
- Renewable Borehole information in surface pump pdf is removed
- Life Cycle Cost is now available in print / product detail in the replacement module
Data
New products:
New product variants:
- Control MPC-EC
- SL, Namreg. Cable length 15 m
What's new in WebCAPS 2012.01?
Software
Renewable
- Water volume field was changed so it’s not changed after user input.
- The calculation of thin film PV modules is improved
- Frequency is removed from renewable surface products.
- Sizing tabels are updated so they now show correct values.
Waste water
- Wrong linking in sizing made ”dry installation” unavailable in sizing. This problem is now corrected.
- Minimum allowed frequency of Waste water pump changed. Will now allow operation down to 25 Hz.
- The main sizing page for Waste water is updated with new default values.
Other changes
- New replacement UI implemented. Will allow users to search for pumps in a google like maner with a search field where characteristica is entered.
- IRR ( Interest rate of retun ) is was added to the life cycle cost calculation
- The option of making a life cycle cost calculation was added to the replacement module.
- CRNE replacement was updated and is now up and running.
Data
New product variants:
- CR-H, CRE-H, CRN-H, CRNE-H
- Hydro Multi-E
- Magna, Namreg
- NB/NBG/NBE/NBGE
- NK/NKG/NKE/NKGE
- TP Mammoth II
What's new in WebCAPS 2011.05?
Waste water
- Added suction side pressure loss in print.
- Pipe calculations changed so the dimension doesn’t have to be in order with the largest dimension first and decreasing size for the following pipes.
- Changed curve viewer to display Curve points correct when a none E-pump is selected.
- Added the possibility of having a negative suction head when sizing.
- When selecting the ”ES” curve the scale is changed to 0 – 1.
Pressure boosting
- Changed the configuration page in pressure boosting sizing.
- The load profile was changed to contain 10 load points instead of 5.
- Added preferred design to pressure boosting sizing.
- Energy consumption pr. year and running time pr year * energy consumption was not matching. The calculation is now changed so they are aligned.
Other Changes
- Changes done to renewable in regards of US units not displayed correct.
- Renewable Solar: Sun tracking problems was not taken into account this is problem is no solved.
- When using WebCAPS with US setup the density within quotation text would still be displayed in SI units. This problem was solved so now density is shown in the correct US unit.
- WebCAPS version number is now included in the bottom of the report pages.
- Cable calculation in groundwater sizing was not calculated, the calculation was changed to output correct cable length.
- In heating the default liquid temperature is changed to lower than the Max temperature.
- The control mode ”temperature control” was changed to displaying correct duty points.
- Updated the WebCAPS help to afflict the current versions and removed WinCAPS specific topics.
- Problems with linking in the Industrial application Maritime were solved.
- Added a link to catalogue in sizing to guide users to right entrance, if they already know what product they want to search information for.
- Minor changes to support Mozilla Firefox 7 were implemented.
- Media for MTS was changed from water to emulsion.
What's new in WebCAPS 2011.04?
In this version of WebCAPS a lot of issues has been solved. A short list of some of the issues addressed in this version can be found below:
- WebCAPS literature search is updated to align search output across product families.
- Updates done to prevent PDF prints from containing other pumps than the one selected in WebCAPS. Modifications have been done to prevent PDF print with the contents of "internal Error".
- Problems regarding pressure losses in pipes for heating applications were corrected.
- Problems with calculation of chamber length for MTR in sizing were solved.
- Double output of each pump in the hit list is now solved.
- Problems with missing roughness in Waste Water pipe loss calculation are now solved. A problem with friction calculation when "Number of pumps in operation" was higher than 1 was also solved
- MTA is now providing a code to determine if the pump has top or bottom suction.
- Sorting of results in hit list is now updated so it also works for "Price" or "Price + energy costs".
- Various changes were made to the pressure boosting area.