Buildings
Industrial solutions
More Industrial solutions
Service & support
Global
Buildings
Industrial solutions
More Industrial solutions
Service & support
An abrasive liquid contains substances, often minerals or inorganic substances, that are harder than the material they rub...
An acceptance test of sprinkler systems is to ensure the functionality and performance of the fire sprinkler system is in...
As “mitigation” means working to reduce greenhouse gases, “adaption” contrasts by focussing the...
In wastewater transport and treatment aerobic means that oxygen is available and that it can be used as an oxidation agent in...
An Air Handling Unit (AHU) is used to re-condition and circulate air as part of a heating, ventilating and air-conditioning...
The function of an air cooler is similar to that of an evaporator. What makes it different is the type of cooling medium it...
A heating system in a building can be based on radiators, convectors, floor heating, air heating or a combination of these....
To prevent corrosion and problems with operation, heating and air-conditioning systems must be constructed so that air can be...
The airlift pump – also called mammoth pump – exploits the increase of the oxygen intake in water under pressure....
Previous | Page 1 / 2 | Next