Buildings
Industrial solutions
More Industrial solutions
Service & support
Global
Buildings
Industrial solutions
More Industrial solutions
Service & support
The difference between inlet pressure and the lowest pressure level inside the pump is called NPSH: Net Positive Suction...
Natural refrigerants have no, or an insignificant, effect on the ozone layer and greenhouse effect. They are widely used in...
A night setback system is used to control a heating system. A night setback system will lower the room temperature at night,...
Nitrile rubber may operate up to about 100 °C. Grundfos uses it in its shaft seals as it has a high resistance to oil and...
The round shape of nodular graphite reduces the stress concentration and consequently, the material is much more ductile than...
A non-return valve allows a medium to flow in only one direction. A non-return valve is fitted to ensure that a medium flows...