FAQ

Showing 71 to 80 of 88 results

Due to the modern design and manufacturing process, the motors currently in use often become hotter during operation than motors used in the past.

Read more...

The EF and SE pumps are equipped with motors cooled by the surrounding pumped medium. In order for the motors to be adequately cooled, the EF and SE pumps must always be completely submerged in the pumped medium during operation.

Read more...

There are several reasons as to why the permitted full load current could be exceeded when operating the pump:

Read more...

Grundfos industrial pumps can be equipped with a wide variety of mechanical seals.

Read more...

The flow switch only causes the MQ to switch off automatically during normal operation if the flow rate drops below 0.07 m³/h.

Read more...

Pure, low-viscosity, non-explosive media without solid matter or long fibres.

Read more...

The MQ is equipped with both an internal flow switch and an external pressure switch.

Read more...

The operating instructions provided with every Grundfos product contain relevant troubleshooting information.

Read more...

The problem may relate to the pressure switch (press control), since deposits can cause it to malfunction.

Read more...

Check to see if the fuse has tripped. Is the power plug plugged in? Plug the pump into a different socket and check to see whether it works.

Read more...