Constant differential pressure, control mode

Constant differential pressure can be used in circulating systems with a pipe system with low pressure loss and with control valves to generate a variable flow.

The pressure drop in the control valves is higher than 50% of the total pressure drop.

  • Heating systems with 2-way valves
  • Air-con system with 2-way valves

    Facebook Twitter LinkedIn Technorati