Intelligent, reliable and efficient district heating systems

District heating systems distribute mass amounts of heat over potentially large areas. And in order to keep the customers happy, three factors are important: reliability, efficiency and intelligence. Grundfos supplies a wide portfolio of pumps to power plants, in boiler houses and in the distribution lines, all combined to ensure that heat is distributed optimally – satisfying all heating demands throughout the district heating network.

Keeping a district heating system running reliably requires attention to detail. Grundfos can help with that. Pressure, flow and temperature are the three main parameters to consider, but water purity and pH-value also play a part in deciding the level of wear and tear in your pipes. However, these parameters can be controlled with a flow filter system and an effective water treatment system, both of which feature Grundfos pumps.