Domestic water pressure boosting

For domestic water supply a water booster pump is designed to increase pressure in a water system in order to provide sufficient water flow and pressure to consumers. Low pressure often occurs in residential buildings during peak system usage, for instance in the mornings and evenings when most people shower and cook. But it also occurs when multiple taps in the home are open, when the home is at the end of the supply line or when there simply is a leak in the mains pipes.