Attention to detail 

A pre-engineered, factory-built booster system built with attention to detail, material choice, components and is functionally verified and tested.  

Dry running protection. The system will stop if there is no water in the pipes and can easily be set up to react to a digital input – for example, from a pressure switch or an inlet pressure measurement. 

Configure standby pumps. The pumps will still alternate automatically to ensure that all pumps run at some stage and no pumps seize up. 

Maximum pressure alarm. A dedicated function monitors the discharge pressure and gives a warning or alarm if a defined limit is exceeded.