News
02-05-2020
Grundfos Expands Quick Ship Program to Large SP Submersible
“We’re improving product availability and positioning stock closer to our partners,” said Matt Barton, Grundfos regional supply chain director. “This new addition to the Quick Ship Program allows us to offer a quick response solution for many of our Large SP submersible applications. Customers depend on Grundfos to deliver quickly during their time of need, and we are here to support them.”
Customers can use the Grundfos Product Center to select the model and size for the application, then check the quick ship list for the in-stock model. Requests for pumps not included in the Quick Ship Program will be handled through the normal quoting process.
Invented in 1967, the Grundfos SP pump was the first ever stainless steel submersible pump. Grundfos’ Large SP submersible pumps are recognized worldwide for reliable performance, superior hydraulic design, high energy efficiency, and long product life. The Grundfos SP is used in applications for water supply, irrigation, foundations, reverse osmosis, dewatering, and groundwater lowering.
Customers can also take advantage of the existing PACO LC Quick Ship Program — and a new addition to Water Utility — that delivers efficient PACO LC end-suction pumps within 24 hours for all stocked kits, 48 hours for all full-assembled pumps, and 72 hours for all kits or pumps requiring custom trim. Shipping times listed are only applicable to qualifying models on the Quick Ship website.
The PACO LC close-coupled end-suction pump comprises of an innovative pump and impeller design that produces up to 91% operational efficiency and provides a wider band of best operating efficiency, even during conditions of off-design operation. The PACO LC is used in industrial, water utility, wastewater, HVAC, plumbing, pressure boosting, and agricultural applications.
For more information on Grundfos Quick Ship Programs, visit https://lp.us.grundfos.com/quick-ship.html.