Hospitals
Never compromise on patient care and safety
Hospitals are complex environments that demand careful consideration for HVAC system design, maintenance and repair. When a HVAC system goes down, surgical procedures can be delayed and other emergency situations rerouted to other hospitals. Older HVAC systems also increase the risk of airborne legionnaires’ disease for patients, which is often caused by bacteria in the water within ventilation systems.
With patient care and safety absolutely paramount, the operating rules for HVAC systems are therefore incredibly strict. Viruses must be prevented at all times, so airflow needs to be constantly renewed. Sanitary risks need to be kept as low as possible, meaning water must have the right quality. And hot water needs to be instantly available, making tap pressure crucial.
This means it’s essential that HVAC and pressure boosting systems can deliver maximum reliability. That they can increase efficiency to reduce OPEX and CAPEX. And that they can ensure a hospital doesn’t have to compromise on the health and safety of both its patients and the environment.
Retrofitting for energy efficiency
When renovating a hospital, a common concern is the compatibility of new systems and the benefits of replacing solutions. But whether the task is upgrading equipment, complying with new regulations or increasing the hospital’s value, it’s essential to keep energy efficiency in mind.
In Grundfos, energy-efficient retrofitting can mean everything from replacing old pumps to transforming the entire system with intelligent solutions that monitor performance.
New hospital project?
At the start of a new hospital project, a number of questions will be asked in relation to HVAC systems since careful planning is critical to integrate and optimise each system. Which pump type is right for the system? Can it be connected to a BMS? And how easy is it to size?
Luckily, Grundfos has a wealth of tools, insights and services to answer these questions and more. We help you select, size, install, commission and maintain your HVAC systems. So you can be sure they meet all your performance needs and provide the best comfort possible.
Can we help?
Are you in the process of finding the right pump solution that meets your requirements? Then Grundfos can help you in the process! Fill in the form below and we will contact you.
Thank you for your request! We will get back to you as soon as possible.
Keep an eye on your inbox, a confirmation email is coming your way!
Click the link in the email to complete the subscription process and you’ll start receiving all the most relevant news and updates from Grundfos. If you don’t complete the sign-up process, you won’t be able to receive our newsletter.
If you’re already subscribed, you will not receive the confirmation email.
Kind regards
Grundfos
Explore our applications and solutions
Every hotel has its own special requirements. But with the right system design, it’s possible to gain complete simplicity and reliability, along with increased water safety and energy efficiency. Grundfos offers a complete range of commercial water pump systems to bring high performance to every hotel. Explore our applications and products below.