Find case

Reset search
Showing 101 to 110 of 373 results
Case banner
New life to an old Hotel
Vilnius, Lithuania: The freshly renovated 22-story Reval Hotel Lietuva offers a warm welcome to international guests travelling either on business, conference or leisure purposes. The hotel is situated on the bank of the River Neris in the centre of Vilnius, only a 10-minute walk from the medieval old town. Many rooms in the hotel have a wonderful view over the old town and River Neris. When the hotel management decided to renovate the hotel, Grundfos was the natural choice as overall pump ...
One small box saves the day - twice - in pump system solution
Shortly after they installed their first Grundfos wastewater pumps and system, the crew at the Rose Creek Wastewater Treatment Plant discovered their usefulness. The MP204 motor protection units saved the plant from disaster one night - a problem that took minutes instead of
One small change in boiler feed level control, one massive change for the better
For the boiler feed level control at Grant’s, Grundfos supplied its CRE 15-8 pumps with built-in variable speed and intelligence.
Optimal comfort in the Igreja da Santíssima Trindade in Portugal
At the Fatima Sanctuary, north of the Portuguese capital Lisbon, lies one of the most important shrines of the world dedicated to the Virgin Mary, The Igreja da Santíssima Trindade (Church of the Holy Trinity). Famous for the apparitions of the Virgin Mary to three shepherd children in 1917, the sanctuary welcomes millions of pilgrims and tourists from all over the world.
Optimised water distribution
Grundfos DDD provides constant and stable water pressure for the end users in Kauniainen in Finland
Patagonian sun turned into water
Large distances are a characteristic factor in the southern end of the Argentinean Patagonia. This makes it a real challenge to install traditional energy sources there. Clean energies solve this problem and many times this kind of solution can even make automatic a daily task.
Polish housing society breaks with tradition
THE POJEZIERZE REGION, POLAND: Polish households spend about 12% of their budgets on energy, compared with an average of 4% in the European Union. The over consumption can be attributed to a combination of thermally inefficient buildings and high distribution losses found in Poland. It is estimated that distribution energy losses in some systems amount to 45% compared with a typical figure of 10% in a well-maintained system. Consequently, there is considerable demand for replacement and ...
Porsche meets Grundfos
WALS-SIEZENHEIM, AUSTRIA: Porsche, manufacturer of prestigious cars, chose a Grundfos solution for wastewater management when its existing service centre was greatly expanded.
Pressurised wastewater transfer protects an environmentally sensitive area in...
The Kållands Vatten & Avloppsförening (Kållands Water and Wastewater Association, a homeowners’ association) located in Lidköping, Sweden, recently embarked on a much-needed upgrade of their wastewater transport system. Grundfos was chosen as supplier and consultant for the refurbishment project, delivering Prefabricated Pumping Stations (PPS) for private homes with SEG AUTO adapt grinder pumps and communication as well as large SLV wastewater pumps at network pumping stations.
Providing professional pump solution for one of Europe’s largest pivot ...
In France some 100 km south of Bordeaux, farmer Jean Claude Briest is the happy owner of one of the largest pivot irrigation system in Europe, and possibly in the world.