Find case

Reset search
Showing 141 to 150 of 373 results
Case banner
Sustainable student housing in smooth waters
For Urban Rigger's floating student homes, Grundfos has supplied MDG Lifting stations to handle the critical wastewater situation, as well as ALPHA2 circulators for heating and SCALA2 for water boosting.
Swedes cheer teamwork, savings in pressurized wastewater network
Sweden’s largest homeowner association faced a challenge. The year was 2012. The area was Lidköping in central Sweden – homes and farms scattered among 100 square-kilometres of rolling hills, lakes, forests and beaches.
The disinfection system Oxiperm Pro
Düsseldorf International Airport (DUS) was opened on April 19th, 1927. Nowadays, it is the most important international junction of North Rhine Westphalia. Düsseldorf Airport is the third largest airport in Germany regarding passenger volume. In total, more than 18.1 million people travel from Düsseldorf to 180 destinations in 50 different countries per year world-wide using 77 airlines (figures from 2008). On average, 49,000 passengers are transported daily on 625 flight movements.
The new buzzwords at this foundry’s paint shop? Data connectivity
For the paint, chemicals and other liquids at BIRN’s CED surface treatment facility, Grundfos has provided a full line of intelligent pumps, monitoring equipment and digital services as part of Grundfos iSOLUTIONS.
The Padania Acque Gestione Drinking Water Supply
The Padania Acque Gestione Drinking Water Supply
The Sagardian Brothers Farm
Located forty miles west of Fresno, CA, The Sagardia Brothers Farm covers 150 acres of rolling hills.
The sensible solution
Situated in the Gerland-District Technopole in the southern part of Lyon, an area that is oriented towards high technology industries, Ecole Normale Supérieure de Lyon (ENS Lyon) is one of the topscientific “ Grandes Ecoles “ in France.
Two-time award winning CR-H offers water treatment facility significant ...
The Olathe Water Treatment Station #2 in Olathe, KS, agreed to participate in a field test and with the assistance of Grundfos Distributor, Pump & Power of Lenexa, KS, the Multi-Stage CR-H was installed in April, 2009 in a backwash application for membrane wash.
Turnkey solutions with intelligent controls bring wastewater pumping stations...
In Aggersund, Denmark, the local municipality decided it was time to update their 40 year old vacuum sewer system.
University campus retrofits heating system, needing 85% less power during ...
University campus retrofits heating system, needing 85% less power during record lows