Direct Sensors™ inside enables a robust and cost-effective water revenue collection platform for the developing world.

Overview_TEXT

Overview

The situation

To start out, the requirements for the GRUNDFOS water revenue collection platform was to ensure a financially viable water supply platform for the developing world – in particular Africa.
The heart of the platform is the innovative water “ATM“(AQtap) and a unique water management system providing a novel modular approach to water supply. From dispensing stand-alone water kiosks at a communal water point to a minigrid of water points in an urban and rural environment. The AQtap needed a very accurate flowmeter, which could lead to a certifiable water “ATM” to secure the correct dispensing of water for payment, and a cost-effective and durable solution which would survive the harsh environments it can be exposed to. Other solutions being tested were either too costly, or not durable in the harsh environment settings with high temperatures and high humidity.

The Grundfos solution

The basic characteristics of the sensor are: without any moving parts, high repeatability and inherent very low drift. The need for higher precision at lower flowrates required the usage of the latest flow-sensor from GRUNDFOS Direct Sensors™. The so called 5th Generation of flow sensors enables a flow accuracy, which, integrated into the AQtap, obtained the OIML R 49-2:2013. Furthermore, the signal from the sensor is used to distinguish between air and water in the system, which is necessary due to frequent air pockets in the deteriorated water infrastructure. The sensors are made in Denmark, but the actual “ATM” unit is assembled and tested in India by GRUNDFOS. 

The outcome

Direct Sensors™ inside enables a robust and cost-effective water revenue collection platform for the developing world. On top of the physical unit an advanced and remote cloud-based, water management system is deployed and integrated with local mobile payment programs. More than 300 systems have been produced to date.

Topic:

Water Dispensing

Location:

Google Map

The developing world – in particular Africa.

Company:

Grundfos

AQtap dispenser unit

AQtap dispenser unit

Related Products_TEXT
Contacts_TEXT

Contact

If you need a similar solution, please contact us for further information.

Contact

If you need a similar solution, please contact us for further information.