Ground Source Heat Pump

app-domestic-ground-source-heat-pump-grey-03

Ground Source Heat Pumps

Grundfos Direct Sensors™ can be used both on the Primary side (ground loop) or Domestic Hot Water / Central Heating sides the GSHP. By measuring the flow and delta T in the system, the SPF(seasonal performance factor) can be calculated. They can help to improve the system through:

  • 2in1 and 3in1 sensors for Flow, Pressure and Temperature Control
  • Leakage control
  • EN1434 Heat-metering and Control (SPF)
  • Enhanced Glycol Flow Performance