Heat-meter solution

HMD

Heat-meter solution

Grundfos Direct Sensors™ VFS (flow + temperature sensor) used in tandem with our RPS (pressure + temperature sensor) will provide the flow, delta T and pressure in the system. By measuring the flow and delta T in the system, the SPF (seasonal performance factor) can be calculated

This can be done for systems ranging from cooling to heating and hot water modules.

Coming soon to the market will be our EN1434 validated flow sensor which will be able to be used in Heat-metering according to the EN1434 standard.
 
For further information on our solutions and the differences between heat-metering, heat-monitoring, and various standards on the market, feel free to contact us.