6 küsimused Baastase

ECADEMY test

Industrial Water Treatment

See kursusetest sisaldab 6 questions and can be retaken at any time.

Testi läbimiseks ja kursuse lõpetamiseks peate vastama küsimustele õigesti.

Alusta testi

Küsimus 2 of 6 Baastase

Put very simple, what are the basics of water treatment?

Küsimus 3 of 6 Baastase

In addition to process water, industries have another type of water that needs treatment. Which?

Küsimus 5 of 6 Baastase

How small particles can an ultrafiltration plant remove?

Küsimus 6 of 6 Baastase

What methods can be used to separate particles and water?

Küsimus 6 of 6 Baastase

Avage MyECADEMY

Esitage oma praegused vastused ja saage testi lõplik tulemus.

Esita

Testi tulemused

Palju õnne. Läbisite testi ja lõpetasite kursuse Industrial Water Treatment

Teenitud märgid:

Jätkake koolitust Avage MyECADEMY

Vabandust. Te ei läbinud testi Industrial Water Treatment test this time

Correct
Q: What is aeration?
A: A process that brings oxygen into the water to get rid of volatile components
Correct
Q: Put very simple, what are the basics of water treatment?
A: Removing or adding content
Correct
Q: In addition to process water, industries have another type of water that needs treatment. Which?
A: Wastewater
Correct
Q: Why is it important to treat water that is to be used in industrial processes?
A: Water can stem from a variety of sources and may contain bacteria, soluble, particles, chemicals or other unwanted substances
Correct
Q: How small particles can an ultrafiltration plant remove?
A: Down to 0,010 µm
Correct
Q: What methods can be used to separate particles and water?
A: Sand filters or membrane technology