6 questions Basic

ECADEMY test

The Extended Basic Hydraulic Principles Course

This course test contains 6 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 1 of 6 Basic

1 Which of the following is NOT a way to reduce friction losses?

Question 2 of 6 Basic

2 Does it create a noise inside the pump when vapourised water molecules implode?

Question 3 of 6 Basic

3 What happens if you double both the pump’s flow and the head?

Question 6 of 6 Basic

6 What should you generally avoid excessive use of when working with pipework?

Question 6 of 6 Basic

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the The Extended Basic Hydraulic Principles Course

Achieved badges:

Continue training Go to MyECADEMY

Sorry. You did not pass the The Extended Basic Hydraulic Principles Course  test this time

Correct
01.
Q: Which of the following is NOT a way to reduce friction losses?
A: Lower the pump inlet
Correct
02.
Q: Does it create a noise inside the pump when vapourised water molecules implode?
A: Yes
Correct
03.
Q: What happens if you double both the pump’s flow and the head?
A: The energy usage is quadrupled
Correct
04.
Q: Why is it an advantage to mount your pump to a fixed base?
A: It helps to keep it steady in bad weather
Correct
05.
Q: What does friction loss refer to?
A: Contact between the moving liquid and its enclosure
Correct
06.
Q: What should you generally avoid excessive use of when working with pipework?
A: Elbows and bends