8 questions Advanced

ECADEMY test

Water Distribution

This course test contains 8 questions and can be retaken at any time.

You must answer all questions correctly to pass the test and complete the course.

Start test

Question 3 of 8 Advanced

3 What is unique about the algorithm used to manage pressure with DDD?

Question 5 of 8 Advanced

5 What is placed in critical pressure points of the distribution network to establish DDD?

Question 6 of 8 Advanced

6 What does DMAs make it easier to localise?

Question 7 of 8 Advanced

7 What must zones be equipped with in order to achieve a fixed constant pressure setpoint at the discharge?

Question 8 of 8 Advanced

8 What is the most efficient way to operate a water distribution system?

Question 8 of 8 Advanced

Happy with your answers?

Submit your current answers and get the final test result.

Submit

Test results

Congratulations. You have passed the test and completed the Water Distribution

Achieved badges:

Continue training Go to MyECADEMY

Sorry. You did not pass the Water Distribution test this time

Correct
01.
Q: What is a result of pressure zoning?
A: The main station and most of the network will operate at a much lower pressure
Correct
02.
Q: What is the general purpose of a water tower?
A: To keep the water in the distribution pipe network pressurised
Correct
03.
Q: What is unique about the algorithm used to manage pressure with DDD?
A: It is self-learning
Correct
04.
Q: How is a DMA created?
A: By closing valves within the distribution pipe network to create a zone and installing flowmeters where valves are left open to register the volume of water supplied and removed from the DMA
Correct
05.
Q: What is placed in critical pressure points of the distribution network to establish DDD?
A: Sensor data-loggers
Correct
06.
Q: What does DMAs make it easier to localise?
A: Leaks
Correct
07.
Q: What must zones be equipped with in order to achieve a fixed constant pressure setpoint at the discharge?
A: A booster pump or pressure-reducing valve
Correct
08.
Q: What is the most efficient way to operate a water distribution system?
A: Using a proportional pressure control system