- Grundfos Indonesia
- Learn
- Ecademy
- All courses
- 62 - The COMFORT range for ...
- Test your knowledge
Question 1 of 4
Intermediate
Where should the COMFORT TA pump and its external temperature sensor be installed?
Question 2 of 4
Intermediate
What is the purpose of a pump in a hot water recirculation system?
Question 3 of 4
Intermediate
How much water can be saved annually with the COMFORT hot water recirculation pumps?
Question 4 of 4
Intermediate
What are the two control modes available in the COMFORT TDT pumps?
Question 4 of 4
Intermediate
Happy with your answers?
Submit your current answers and get the final test result.
Test results
Congratulations. You have passed the test and completed the 62 - The COMFORT range for hot water recirculation systems
Sorry. You did not pass the 62 - The COMFORT range for hot water recirculation systems test this time
Achieved badges:
How would you rate this course?
1: Where should the COMFORT TA pump and its external temperature sensor be installed?
The COMFORT TA pump must be installed on the return line, and the external temperature sensor must be installed on the return line next to the pump
You can find the answer here >
1: Where should the COMFORT TA pump and its external temperature sensor be installed?
The COMFORT TA pump must be installed on the supply line, and the external temperature sensor must be mounted on the return line
You can find the answer here >
1: Where should the COMFORT TA pump and its external temperature sensor be installed?
The COMFORT TA pump must be installed on the return line, and the external temperature sensor must be mounted on the supply line
2: What is the purpose of a pump in a hot water recirculation system?
It creates sufficient water flow to compensate for heat loss in the pipeline
2: What is the purpose of a pump in a hot water recirculation system?
It helps a booster pump ensure sufficient water pressure in taps
You can find the answer here >
2: What is the purpose of a pump in a hot water recirculation system?
It performs both listed tasks above
You can find the answer here >
3: How much water can be saved annually with the COMFORT hot water recirculation pumps?
Up to 7,500 gallons or 34,050 litres
You can find the answer here >
3: How much water can be saved annually with the COMFORT hot water recirculation pumps?
Up to 5,000 gallons or 22,700 litres
You can find the answer here >
3: How much water can be saved annually with the COMFORT hot water recirculation pumps?
Up to 10,000 gallons or 37,850 litres
4: What are the two control modes available in the COMFORT TDT pumps?
AUTOADAPT and Temperature control mode
You can find the answer here >
4: What are the two control modes available in the COMFORT TDT pumps?
Temperature control mode and Timer
4: What are the two control modes available in the COMFORT TDT pumps?
AUTOADAPT and Timer
You can find the answer here >