Research And Insight

Initial costs (Cic) for pump systems

In the calculation of lifecycle cost, the initial cost of a pumping system covers all the equipment and accessories needed to operate the system. 

Initial costs include the purchase of: 

    • Pumps 

    • Frequency converters 

    • Control panels 

    • Transmitters 

The initial costs may conceal the real cost of an installation over its lifetime. 

There are certain trade-offs that should be seen in this context. For instance, a speed-controlled pump system may use considerably less energy compared to a cheaper constant-speed system. Over its lifetime the energy saving can more than offset the higher initial cost. 

The graph compares the initial cost of a constant-speed pump system (system 1) with a speed-controlled pump system (system 2). The higher initial cost of a speed-controlled pump is often offset by lower operating costs. 

Use the Grundfos sizing tool to ensure a realistic basis for calculating initial costs for the complete pump system. 

Related products

Find products from Grundfos related to this subject.

Related applications

Find applications from Grundfos related to this subject.