Research And Insight
Sprinkler distribution pipework
The sprinkler pipework distributes the fire suppression media, typically water, into the different building areas. The pipe system design must be in compliance with the specifications described in the installation standard for fire sprinkler systems, and these specify the system design and components required.
The pipe material must be protected against corrosion, and specific materials are typically preferred for specific installation types. The following pipe materials are used, and they must be produced in compliance to typically a DIN standard.
- Ductile cast iron
- Black steel pipes
- Galvanized steel pipe
- Pressure pipes made of polyethylene or polyvinyl chloride
- Stainless steel pipe
Pipes must be installed for easy repair and not embedded in ceilings or concrete floors. They must be protected against mechanical damage and non-galvanised steel pipes must be painted – normally in a red colour.
Mechanical pipe joints must typically be approved by a 3rd party approval body. Flexible joints also called compensators/expansion joints are used to absorb pressure shocks or minor relative movements between two pipes – but are not to be used in case of misalignment between pipes.
Pipe supports have to be fixed directly to the building and may not be used to support any other installation.
Grundfos supplies fire pumps for water supply as part of approved fire sprinkler systems for industrial and commercial fire protection.