News
26-05-2020
Grundfos India’s facility receives the prestigious ‘LEED Platinum’ certification
Chennai, May 13, 2020: Grundfos India, a global leader in advanced pump solutions and a trendsetter in water technology, today announced that its India facility in Chennai,
comprising of both its country headquarters and the factory building, has been accredited with LEED Platinum Certification by the U.S. Green Building Council (USGBC). This is the highest level of rating offered by Leadership in Energy and Environmental Design (LEED) for green buildings and is a global benchmark for environmentally-responsible designs and sustainable construction practices.
Sustainability is becoming even more critical in the current scenario with natural resources such as water and energy rapidly depleting. Grundfos has been one of the early adopters in implementing measurable green strategies and exhibiting the highest standards of water and energy conservation, waste management, CO2 emissions, environmental quality and occupant satisfaction. The renewal of LEED certification for the entire facility reinforces Grundfos India’s commitment to champion sustainable initiatives. The company received an overall score of 84 points for its facility, which spreads across 1,48,758 square feet.
“Achieving the LEED Platinum certification for our factory underscores our efforts to meet effective corporate green strategies. This now means that our entire facility, both the office and factory is Platinum rated. Sustainability is an integral part of our ethos and business model, and we believe our buildings should embody the values that we believe in” said Saravanan Panneer Selvam, General Manager, Grundfos India.
The Grundfos India facility has underground water tanks with the capacity of 3,50,000 liters to harvest rainwater that helps collect 53% (approx.) of precipitation. In addition to this, all the wastewater from the factory is being recycled and is made available for landscaping and gardening purposes, making it a zero-liquid discharge (ZLD) facility. The building also has a provision to collect and condense water from Air Conditioners for reuse.
With its sustainable green building design, the facility optimizes natural daylight and also has efficient lighting and air conditioning systems to reduce its energy consumption. It also has a solar photovoltaic installation in the roof-top that generates about 208 Mwh per annum that is used within its facility, further contributing towards reducing its CO2 emissions.
Grundfos India’s headquarters in Chennai (office building) was the first commercial building in the country to be ‘LEED Gold’ certified in 2005. Persistent efforts to achieve the highest levels of sustainability encouraged the company to apply for voluntary recertification of this building in 2013 when it was elevated to a Platinum rating. Now with its factory also receiving this rate, the entire premises is LEED Platinum rated.
About Grundfos India
Grundfos Pumps India Pvt. Ltd. (Grundfos India) a wholly-owned subsidiary of Grundfos Holdings was established on March 13, 1998. Grundfos India is responsible for sales of Grundfos products in India, Bangladesh, Bhutan, Nepal and Maldives. Currently, Grundfos India has more than 400 employees and works with 200 distributors and dealers with 26 offices across India. Grundfos India provides energy-efficient pumps and smart pumping solutions for various applications – heating and hot water service systems, cooling and air-conditioning systems, industrial applications, pressure boosting and liquid transfer, groundwater supply, domestic water supply, sewage and wastewater, dosing, chlorination systems, disinfection systems and pumps running on renewable energy.