BioBooster cleans up in Norwegian municipality

Hemsedal - Retrofit

Grundfos’ retrofit solution at Ulsaak wastewater works for Hemsedal municipality, Norway.

The extension was constructed to accommodate the Grundfos solution. The solution comprises two filter modules and a supply module. The extension was commissioned in 2012. Treatment capacity: 17 m3/time (75 gall/min).

The first municipal wastewater treatment plant in Norway with a membrane bioreactor is ensuring that increased wastewater at a tourist hot spot is efficiently managed and that the vital fishing river remains clean.