Research And Insight
A paradigm shift in chilled water systems
Grundfos Distributed Pumping marks a paradigm shift in chilled water systems
towards a new era of decentralised pumping. This new pumping principle is ready to meet the growing cooling demand by taking building comfort and efficiency to new levels.
Why Distributed Pumping is needed
The global cooling demand has doubled in less than 20 years
Global use of energy is projected to increase almost 25% by 20501. And in the past 20 years, the global cooling demand alone has nearly doubled, making it critical to rethink chilled water systems and improve energy efficiency.
Distributed Pumping has the potential to save up to 54% energy
Many buildings operate with centralised and inefficient chilled water systems. Replacing balance and control valve with distributed pumps can reduce total pump energy consumption for a chilled water loop by 54%, amounting to substantial energy savings2.
Around 45% of chilled water pumps run at peak-load most of the time
It’s estimated that 45% of pumps within chilled water systems are running constantly at peak-load3. Yet this level is rarely needed since chilled water systems only operate at peak consumption a very small fraction of the time – roughly 1-3%.
A new era of decentralised pumping
Many buildings are running inefficient chilled water systems, causing overpressurisation and low Delta T. This is often caused by poor comissioning and low efficient pump management. Watch this video, to learn how Grundfos Distributed Pumping can minimise energy consumption and maximise indoor comfort.
The typical challenges
When it comes to chilled water systems, many buildings are still working with inefficient, decade’s old solutions. As a result, these systems will typically experience a number of challenges, such as poor pump control, low Delta T, difficulties complying with building energy codes, as well as complexities in design, installation and commissioning.
Inefficiency occurs when pumps sized for full system flow and maximum pressure loss operate at too high a speed. This then results in over-pressurisation and low Delta T. Control and balancing valves therefore have to throttle the flow and pressure, which is like controlling the speed of a car with a handbrake.
Inadequate commissioning and poor pump control also lead to imbalanced systems and excessive energy use. And it’s not only energy waste that’s the problem; indoor comfort for occupants is also compromised. On top of this, there’s the risk of penalties if energy consumption requirements aren’t fully complied with.
How you can optimise
When optimising energy efficiency in buildings, the focus is often on energy creating systems such as boilers and chillers. However, as energy distribution has a significant impact on overall energy consumption, an increased focus towards energy distribution is necessary.
A system can utilise intelligent pumps on each floor of a building to achieve this optimal energy distribution – eliminating the need for valves in the building since the pressure is provided only when and where it’s needed.
Replacing valves with pumps will ensure optimal pressure and flow to each terminal unit at all times. This kind of demand-driven system enables easy commissioning, an automatically balanced system throughout a building’s lifetime, improved Delta T, seamless integration and minimum pump pressure. All of which means significantly reduced energy use.
The solution
Grundfos iSOLUTIONS offers a new pumping principle for chilled water systems called Distributed Pumping. It requires no control-, balancing- or PICV valves since these are replaced by smaller intelligent pumps such as the Grundfos MAGNA3. The overall pressure in the system is therefore significantly lower as each pump generates only the amount of pressure needed.
In addition to this, the large primary pump is exchanged with a smaller, intelligent pump such as the Grundfos TPE3, enabling significant CAPEX savings. These intelligent pumps are connected to sensors so that operation adjusts to the demand. And this system design results in substantially lower energy usage and total expenditures.
Ultimately, Grundfos Distributed Pumping is the most efficient way of circulating chilled water in HVAC systems today. It’s able to take building comfort and efficiency to new levels, saving OPEX, commissioning time and energy. So, with Grundfos Distributed Pumping for commercial buildings, you can fully control a chilled water system, minimise energy and costs, and ensure a much more comfortable indoor climate.
Podcast: Grundfos Distributed Pumping
Grundfos Business Development Manager Pete Korzeniewski is our guest today. Pete’s an expert in HVAC efficiency and Distributed Pumping. He explains how we should shift our focus from energy creation to energy distribution in order to make commercial buildings run more efficiently.
You can listen to more podcasts from Grundfos Commercial Building Services - on your preferred platform.
Explore Distributed Pumping solutions
Grundfos Distributed Pumping makes it easy to balance chilled water systems and enhancing comfort in buildings. The solution replaces traditional balance and control valves with intelligent pumps.
54% energy savings
Grundfos Distributed Pumping helped Ngee Ann, a large university building in Singapore, increase Delta T by 28% and reduce total pump energy by 54% – all while providing optimal comfort for building users.
SOURCES
Source1: Global cooling report; International Energy Agency, June 2020 https://www.iea.org/reports/cooling
Source2: Grundfos Case Ngee Ann Polytechnic (Polytechnic Block 22), energy savings calculation of Distributed Pumping compared to conventional system
Source3: Seasonal load changes, when calculating Energy Efficiency Ratio EER and Integrated Part Load Value IPLV for chilled water systems
Related applications
Find applications from Grundfos related to this subject.
Other related articles and insights
Find related articles with research and insights from Grundfos.