Encyclopedia search

Reset search
Showing 361 to 370 of 398 results
Subcooling
Subcooling is a technical expression for a refrigerant in liquid phase at a temperature lower than the corresponding evaporating temperature to the actual pressure.
Submerged installation
The two most common installation types are free standing pump installation and pump installation on an auto coupling.
Submersible pump - clean water
A submersible pump is a unit combining a pump and a motor to an enclosed unit, suitable for submerged installation. The pump comes in both a single-stage and a multi-stage version
Suction lift
Suction lift refers to the pressure (negative pressure) on the suction side of the pump.
Suction superheater
The purpose of the suction superheater in a cooling system is to protect the compressor from liquid drops, and to increase the evaporating section of the evaporator.
Superheating
Superheating is a technical expression for a refrigerant in gas phase at a temperature higher than the corresponding evaporation temperature related to the actual pressure.
Suspended solids
Particles which remain in suspension in water are called suspended solids.
System characteristic
The system characteristic describes the connection between volume flow-rate and pressure loss in a given pipe system.
System characteristics
The system characteristics show the pressure loss in the system as a function of the flow
Tandem seal
Tandem seal is Grundfos’ name for a shaft seal system, where an additional sealing chamber has been mounted on the existing shaft seal.