Possible cause of fault
Automatic night set-back is active
The hydraulic conditions have changed. The pump must adapt to these.
When night set-back is activated
Switch on night set-back using button 3.
In "AutoAdapt" mode
Possible cause of fault: The "AutoAdapt" function is unable to correctly adapt the heating system.
Remedy
Switch off the pump for 5 minutes using the power switch on the electrical supply line (not the switch on the pump) and then switch back on.
Use button 3 to cycle through the possible curves until "AutoAdapt" has been reactivated. The automatic setting may need up to a few hours to adapt to the system curve.
If this measure does not lead to the desired outcome, the pump can be configured to (specific) curves.
Remedy
Begin by using button 3 to cycle through the possible proportional and constant pressure curves, testing each setting for approximately two hours.
If there is no increase in the heat supply, please call your specialist technician.