Case

SINGLE Temperature Control Systems

The Situation

Sensors for “Temperature Control Systems” based on water

“Single is a manufacturer of heat-balancing technology, including surveillance controls and manifolds. Single needs to measure, display and control the flow and temperature in their different temperature control systems.”

Single Temperiertechnik Gmbh (Single, ed.) is one of Grundfos largest CR customers world wide. As a secured Grundfos client in Germany for pumps, it was naturally for the IEM sales team in Germany to open the door for Grundfos Sensor A/S to hear, whether Single could have an interest in the Grundfos Direct Sensors™.

Single have been looking for years at a cost-effective way to measure the flow and temperature in the temperature control systems. The intention was to find a sensor solution without moving parts, which can withstand in the different applications at Single.

The purpose of measuring the temperature is to keep a constant return temperature from the processes, and set of the flow depending on the task being performed.

 

The Grundfos Solution

The presentation at Single was actually focusing on another sensor to be used in conjunction with CRE pumps. It was then that the Electrical Engineer at Single felt in love with the concept of the flow sensor having no moving parts. The price from Grundfos was very competitive compared to similar solutions, and having the temperature integrated came as a bonus. This was a must-have and short time after, the first order for flow sensors were issued to Grundfos. 3 months after the visit, Single had found a solution of how to integrate the flow sensors into the temperature control systems and made small alterations to the controls to be able to receive the signal from the Grundfos Direct Sensors™.

In the middle of March 2006 the first units were shipped from Single, and are now operational at various machine tool manufacturers.

The applications for our flow sensors are never ending, as we have a cost effective solution for a lot of applications, where only a flow sensor without any moving parts will be able to do the job. Water cooling units is an interesting applications area for our Grundfos Direct Sensors™, as we have a combined flow and temperature sensor, which limits the sensor and installation cost for the Grundfos Industrial OEMs.

Gunther Drews, Sales Manager, Grundfos Direct Sensors

 

The Outcome

The advantages of the Grundfos Direct Sensors™ could be used in several ways at Single. The combination of flow and temperature in one unit enabled Single to integrate the sensor also in crowded systems. The sensor principle without moving parts assured reliability and robustness in harsh environments. And the competitive price makes it possible to integrate sensors also in low cost temperature control systems.
Since March 2006, Single has been a customer of not only pumps but also for the Grundfos Direct Sensors™. The sensors have been integrated in different other applications at Single through the last couple of years. 

Grundfos Direct Sensors™ have been established as standard in a lot of applications at SINGLE. With now about 1500 sensors in the field we are satisfied with the accuracy and reliability.

Johannes Kübler, Quality Manager SINGLE

Other related cases 

Read related stories from customers who have also benefited from a Grundfos solution.