Case

Integrated solution for mixing loops - Smart mixing with cloud monitoring

It is much easier to use this kind of mixing loop as a complete solution instead of having to design and install each component individually. The seamless interaction between the control unit and the pump is also a huge advantage.

Alexander Grafe, Technical Director at OVE Property Supply with Efficient Use of Energy

"When it comes to heat contracting, it is crucial for us to be able to precisely monitor and constantly optimise the operation of our plants. That is why we started looking at innovative solutions for mixing loops early on", says Alexander Grafe, Technical Director at OVE Property Supply with Efficient Use of Energy. The medium-sized energy contracting company takes a comprehensive approach when it comes to supplying neighbourhoods with energy in an innovative and sustainable way, with already more than 450 properties nationwide.

OVE learned about MIXIT, the mixing loop solution by Grundfos, back in 2017. "The all-in-one solution with integrated pump control was exactly what we needed", recalls Alexander Grafe. "We talked to Grundfos at a trade fair and a short while later we had completed our first project with MIXIT." There are now more than 30 plants in operation. OVE is now using the latest MIXIT generation, launched by Grundfos in the spring of 2021.

 

Reference property with the latest MIXIT generation

The first OVE project to use the new MIXIT generation is a housing estate in Bad Rothenfelde and the contracting provider is also using it as a reference property. The property completed in 2021 features eight housing units and another eight units are to follow in the second building phase in 2022. The supply technology has already been designed for all 16 housing units.

Heat is primarily generated by a gas-powered CHP unit. The de-coupled heat of 70-85 degrees is buffered using a phase-change memory to ensure optimal service life for the CHP unit. The units are supplied using a low temperature circuit, which is designed to keep the flow/return at 45/35 degrees all year. To do this, each unit has its own transfer station with an underfloor heating manifold and a combined electrical flow heater to support peak loads when heating domestic water.

"Creating our mixing loop with a complete solution, instead of having to lay out and install all the components individually, is considerably easier. The seamless interplay between control unit and pump is also a decisive advantage." Alexander Grafe

Mixing loop for flow adjustment

A mixing loop with Grundfos MIXIT ensures that the flow is lowered to the level of the supply circuit. To do this, part of the return flow from the supply network is added to the 60 to 70 degree flow. The return is at a temperature of about 25 to 30 degrees and the required temperature for the supply circuit is around 40/45 degrees.

"Naturally, it is much easier to use this kind of mixing loop as a complete solution instead of having to design and install each component individually", says Alexander Grafe. "And the seamless interaction between the control unit and the pump is a huge advantage. The control unit controls the operation of the pump and also uses its sensors. All you have to do is parameterize the control unit and not each individual component. The bottom line is that the solution makes it extremely easy to precisely adapt the flow and to find the optimal Delta T (spread of flow and return temperature) for efficient operation."

Monitoring with the new cloud solution

The plant is monitored remotely from the control room at the company headquarters. To make this possible, the latest MIXIT generation is equipped with its own RJ45 input, allowing you to monitor the mixing loop using the Grundfos cloud solution, BuildingConnect. This platform is used to monitor, control and operate heating systems in smaller properties that do not have comprehensive control technology. While important functions can be used in the MIXIT standard version, the complete scope of functions requires a software upgrade for the control unit.

"The cloud solution is an important advanced development for mixing loops", says Alexander Grafe. "With older models, we used the GENIbus protocol to access the data. Now with the cloud solution, all we need is an active internet connection to have visualized access to all of the mixing loop's data points via the dashboard at the factory."

OVE plans not only to use the latest MIXIT technology in new plants, but also when modernizing old plants. "The all-in-one solution has proven itself to us in dozens of plants", states Alexander Grafe. "It reduces the cost of planning and installation, is easy to handle and gives us maximum control over the mixing loop operation. The cloud monitoring solution for the latest generation is a meaningful development and has made the concept even more attractive to operators looking to consistently optimize their plant."

The cloud solution is an important further development for mixing loops. All we need is an active internet connection for visualized access to all of the mixing loop's data points via the dashboard at the factory.

Alexander Grafe, Technical Director at OVE Property Supply with Efficient Use of Energy

All-in-one mixing loop

Grundfos MIXIT is an all-in-one mixing loop with flexible offerings and features designed to accommodate every need in heating systems. MIXIT has a built-in actuator, controller and sensors, making designing, installing and operating mixing loops simple and easy.