FAQ
Question: Can the SP pumps also be operated in a horizontal position?
Answer:
SP submersible pumps with a Grundfos or other submersible motor can be operated in any position from horizontal to vertical. The motor is arranged below the pump. A cooling jacket is generally required for these installation positions.
Additional information:
Other related FAQ
Find other frequently asked questions related to this subject.