News
Grundfos go beyond the pump
07-Jan-2019
Efficiencies are a function of good pump design and not purely a standalone benefit, so it is important to understand the true value of pump efficiency. This means that to achieve the highest overall efficiency the complete installation needs to be examined as opposed to just viewing the pump in isolation and being able to deliver real energy savings with a short return on investment.
By thinking beyond the pump and taking the entire pumping system into account it is possible to optimise the way pumps, drives, controls & protection, measurement and communication units work together as part of one system. A manufacturer like Grundfos, can incorporate specific demands with their application expertise. They can then take these requirements and translate them into state-of-the-art pump intelligence - for any application. This approach that is both integral as well as encompassing the integrity of the entire system and is called Grundfos iSOLUTIONS.