FAQ
Question: Why there is no sensor for chemical tank monitoring in SMART Digital CHEMPAIRING Suite?
Answer:
We have asked our customers about the best sensor principles to measure the tank volume for interchangeable chemical containers (from 10L canisters up to IBC). None of the sensor principles (e.g., internet-connected scale, ultrasonic, radar) really convinced our customers. Most of the time they are expensive, need a time-consuming calibration procedure, can only show the level but not the volume, and disappear with the container exchange. Therefore, we concluded that the best sensor for interchangeable containers is no sensor.
Additional information:
Frequently Asked Questions
Where can I operate SMART Digital CHEMPAIRING Suite?
The cloud solution is made for stationary installation in the following countries:
North Americas
- USA
- Canada
Nordics/Baltics
- Denmark
- Sweden
- Finland
- Norway
- Estonia
- Lithuania
- Latvia
DACH
- Germany
- Austria
- Switzerland
East Europe
- Poland
- Hungary
- Czech Republic
- Romania
- Slovakia
- Slovenia
- Croatia
- Serbia
- Bulgaria
South Europe
- France
- Italy
- Greece
- Spain
- Portugal
Benelux/UK&I
- Great Britain
- Ireland
- Netherlands
- Belgium
- Luxembourg
How much will it cost to operate SMART Digital CHEMPAIRING Suite?
With less than EUR 1 per day for up to 3 systems per installation (a system = 1 DDA dosing pump with one gateway), you get the full benefit of SDCS. An annual subscription plan will lower the billing cost for your organisation and you can implement the cost in the annual service plan that you have with your customer.
Why doesn’t a remote control task happen in a few milliseconds in SMART Digital CHEMPAIRING Suite?
Dosing applications are critical, which is why we’ve implemented a feedback loop in the remote-control process. When you send one or more commands to the dosing pump via our web portal, we temporarily save your desired settings, send the commands to the pump and block the input page. After a few seconds, we query the pump to confirm it has accepted the settings. We then compare your desired settings with the accepted ones and provide feedback to ensure the pump operates with your specified settings. This procedure guarantees that the dosing pump operates as intended.
Why there is no sensor for chemical tank monitoring in SMART Digital CHEMPAIRING Suite?
We have asked our customers about the best sensor principles to measure the tank volume for interchangeable chemical containers (from 10L canisters up to IBC). None of the sensor principles (e.g., internet-connected scale, ultrasonic, radar) really convinced our customers. Most of the time they are expensive, need a time-consuming calibration procedure, can only show the level but not the volume, and disappear with the container exchange. Therefore, we concluded that the best sensor for interchangeable containers is no sensor.