News

Grundfos helps combat global warming

Typically, existing pumps are D-labelled. Replacing them with new Grundfos A-labelled products can mean huge energy savings. A-labelled circulator pumps use up to 80% less energy than D-labelled pumps, and can cut up to 10% off an average household’s energy bill.

The internationally recognised independent organisation Europump estimated that changing all the D-labelled pumps in Europe to A-labelled models would save 44 billion kWh every year. That's the same as the total power output of five nuclear plants.

Together with Grundfos, our customers can make this happen for the safety and future of our planet.

> moderncomfort.grundfos.com