Research And Insight

Expansion of fluid

When a liquid is heated it expands, its density falls as temperature increases. The temperature of a liquid in a heating system will vary significantly over time. Typically, this can be between 20-80 °C, which will cause an increase in volume in the hot water heater expansion tank of approximately 3 %. Each heating system must be designed to accommodate its specific expansion requirements.

There are two types of heating system expansion systems: Open expansion and closed expansion tanks.

Open expansion

Open expansion is a system where each boiler is connected to the outside atmosphere by a safety conduit. The safety conduit must never be closed.
The safety conduit can be directed over the roof, either via an expansion tank or directly.

Closed expansion

A closed system is a system where expansion is absorbed in a pressure expansion tank. The expansion tank is usually fitted with a diaphragm that separates the liquid from the air in the tank. The closed expansion system must also be fitted with a relief valve.

Solid-fuel systems are typically fitted with open expansion on the primary side and a closed expansion on the secondary side.

Grundfos CR pumps are typically a part of boiler and heating systems requiring a boiler expansion tank or a hot water expansion tank.

Related products

Find products from Grundfos related to this subject.

Related applications

Find applications from Grundfos related to this subject.