Case

Grundfos KPL Stormwater Pumps Play Instrumental Role in Florida Everglades Restoration Project

Grundfos Pumps Help Move Water From Lake Okeechobee to the Everglades Agricultural Area Stormwater Treatment Area For Cleaning, Storage; Project to Provide Clean Water to the Everglades, Coastal Communities, Aquifers

The EAA Reservoir and Stormwater Treatment Area is a triumph in sustainable design that will positively impact Florida’s residents, the local economy and the native wildlife for generations.
Jack Canfield, Market Development Manager of Water Utilities at Grundfos

Grundfos Pumps Help Move Water From Lake Okeechobee to the Everglades Agricultural Area Stormwater Treatment Area For Cleaning.

Grundfos a global leader in water technology and services, announced today that the Grundfos KPL submersible axial flow propeller pumps are installed in multiple pump stations in the Everglades Agricultural Area (EAA) Stormwater Treatment Area. With the ability to pump 146,000 gallons of water per minute, Grundfos KPL pumps will move water from Lake Okeechobee into the 6,500-acre EAA stormwater treatment area and reservoir for storage and cleaning. The clean water will then move south to nourish the Everglades and replenish Florida’s aquifers and the Florida Bay.

 

“The EAA Reservoir and Stormwater Treatment Area is a triumph in sustainable design that will positively impact Florida’s residents, the local economy and the native wildlife for generations,” said Jack Canfield, Market Development Manager of Water Utilities at Grundfos. “Grundfos’ role in this project exemplifies the company’s belief that everyone deserves access to clean, safe water, including the local ecosystem of birds, fish and plants. We are proud to work with the South Florida Water Management District, the engineers at Brown and Caldwell, and the construction team at Phillips & Jordan to ensure the success of a hydrological restoration project of this scale and complexity.”

For decades, toxic runoff from agricultural land use entered Florida’s canal system and made its way into natural waterways, lakes and coastal communities. In 2019, Florida Governor Ron DeSantis enacted an ambitious Everglades restoration project that includes the EAA Reservoir and Stormwater Treatment Area, which will use the natural filtration systems of the Everglades to reduce harmful discharges like green algae and other bacteria and restore the natural flow of clean water to South Florida.

Grundfos KPL submersible axial flow propeller pumps are installed at two pump stations within the stormwater treatment area. One pump station is now operational, and the other is completing the testing and analysis phase while power is connected to the station.

“The entire Grundfos team feels immense pride as we see this critical phase of the Everglades restoration project come to fruition,” said Hamed Heyhat, EVP & Divisional CEO of Water Utility at Grundfos. “As stewards of our environment and a global leader in water solutions, we recognize the critical role water plays in sustaining life and ecosystems. The installation of these Grundfos solutions marks a significant step forward in our commitment respect, protect and advance the flow of water. Through innovative technology and collaborative efforts, we aim to ensure a brighter, healthier future for generations to come.”

Grundfos KPL Submersible

Grundfos KPL submersible axial flow propeller pumps are designed for high flow and low head water movement, making them ideal for flood control, irrigation, and other large-scale water management applications. These pumps are known for their efficiency, reliability, and the ability to handle large volumes of water. The axial flow design allows for the movement of water in a direction parallel to the pump shaft, optimizing hydraulic conditions and minimizing energy consumption.

The KPL series features robust construction and can operate under challenging conditions, including handling of lightly contaminated water. These pumps are equipped with propellers that are specifically designed to ensure the highest efficiency and durability. They also come with various control and monitoring options that can be tailored to specific needs, providing operational flexibility and ease of use.

Grundfos's commitment to innovation is evident in the KPL series, which incorporates advanced materials and engineering techniques to extend pump life and reduce maintenance requirements. This makes the KPL pumps not only a powerful solution for managing high water volumes but also a cost-effective choice for large-scale water applications.

Grundfos KPL submersible axial flow propeller pumps are installed in multiple pump stations in the Everglades Agricultural Area (EAA) Stormwater Treatment Area.

 

About Grundfos

Since 1945, Grundfos has been committed to pioneering solutions to solve the world’s water and climate challenges and improve people's quality of life. Owned by the Grundfos Foundation (Poul Due Jensen Foundation), the company’s products for Commercial Building Services, Domestic Building Services, Industry and Water Utilities are sold in a large number of countries by local distributors. Grundfos believes that achieving diversity in the company’s workforce and talents, for instance, in terms of gender, ethnicity and work capacity, is essential to the company's progress. Grundfos is a multi-national company with global headquarters in Denmark and the U.S. Main Office and Global Headquarters for Water Utility in Brookshire, Texas. For more information, visit https://www.grundfos.com/us and connect on LinkedIn, YouTube, Facebook and Instagram.