In recent years, the cost of generating clean energy from renewable sources has decreased sharply. At the end same time, governments around the world are recommending that a greater proportion of energy is generated from a renewable source. 

SQFlex solar submersible pumps from Grundfos present cost-effective, flexible and secure water supply solutions using clean energy.

For more information on Grundfos solar solutions:


See how Grundfos solar solutions have helped our communities in tough times

Grundfos Solar SQflex pumps helped communities of West Bengal with optimised grid-independent pumping solutions based on renewable energy, serving as a ray of hope in the aftermath of the Amphan cyclone.

  

Increase your peace of mind with SQFlex

With its built-in electronics, SQFlex offers improved reliability and pump operation, giving you peace of mind. SQFlex features Maximum Power Point Tracking (MPPT) – a built-in electronic unit which continuously optimises the duty point of the pump according to the available input power.

Sustainable solution

SQFlex uses renewable energy sources such as wind and solar, making it one of the cheapest submersible groundwater pumps when it comes to operating costs. 

Intelligent system

SQFlex is more than just a solar pump – it is a complete intelligent system, as its built-in electronics make it compatible with both AC and DC power supply.

Perfect for your application

It can be customised to match your application and local conditions perfectly and it is remarkably easy to install.

Grundfos India in collaboration with Span Pumps, a system integrator of solar solutions enabled community water supply for the village of Gauramwala, in Maharashtra. 

  

Grundfos SQflex enabled drinking water supply for a population of 600 to 700 people in a rural village in Madhya Pradesh. The solar pumps installed at the site could pump about 20,000 litres of water per day from an open well and supply to the community.